This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH983-Q1: 90HH983 Internal Pattern Generation

Part Number: DS90UH983-Q1


Hi team:

Thank you for your support.

I would like to inquire about the Internal Pattern Generation feature of the PDS90HH983-Q1 Serializer with DSC compression.

My display resolution is 6400180090Hz (RGB888, blanking: 1.2). The Deserializer used is HH984, utilizing DSC 1:3 decompression. Can I use the Internal Pattern Generation feature of the HH983 Serializer to generate an Internal Pattern that matches this screen resolution (6400180090Hz (RGB888, blanking: 1.2)), and compress it using DSC 1:3, and then send the compressed data via FPD-LINK to the HH984 Deserializer to drive the display? Is this technically feasible?

Best wish

Zhaomeng