• TMS320F28377D: sysconfig进行系统配置 ,目前存在一些不完整或者是局限性吗?

    Part Number: TMS320F28377D
    Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
    一般使用sysconfig进行系统初始化配置,对于时钟树这一块仅仅是生成了一个clocktree.h文件吗,
    一般使用sysconfig生成的board_init在device_init后调用,
     
     
    device_init进行相关sysctrl初始化,包括flash,clock等,当然还有很多其他内容,

    我想表达意思是:sysconfig可能对应了全部芯片配置…
  • LAUNCHXL-F28379D: 对于中断嵌套的疑问

    Part Number: LAUNCHXL-F28379D
    Other Parts Discussed in Thread: SYSCONFIG, C2000WARE

    Ti的工程师们你们好

    我想请问一下要如果想要使用中断嵌套的话除了设置中断还需要做什么操作呢?或者说有没有结合sysconfig进行中断嵌套设置的一些教程呢?我使用sysconfig进行中断设置时只要设置多个中断时就会出现中断冲突,因此我想试试看中断嵌套能否解决这个问题

    TRANSLATE with x
    English
  • TMS320F280039C: 无法实现中断嵌套

    Part Number: TMS320F280039C
    Other Parts Discussed in Thread: SYSCONFIG, TMS320F28388D, C2000WARE

    我配置了三个定时器中断,定时器周期都是固定1s中断一次,timer0、timer1、timer2中断,我想让timer2在执行中断程序的时候可以被timer0打断,代码如下,基本是按照官方给的参考文档完成的,但是这样并不能实现中断嵌套,这是为什么

    interrupt void INT_myCPUTIME…
  • TMS320F2800157: 2800157 将库函数函数指定位置存放

    Part Number: TMS320F2800157
    Other Parts Discussed in Thread: C2000WARE

    在2800157 中如何将FAPI_F280015x_EABI_v2.00.10.lib库中的Fapi_issueProgrammingCommand(),Fapi_issueAsyncCommandWithAddress()等函数放置在ram区域,也就是编译完成后,函数的存放地址在RAM区域,断电后这两个函数不会保留在程序中

  • TMS320F28035: Flash_Verify(Flash_ptr,Buffer,Length,&FlashStatus);操作失败

    Part Number: TMS320F28035
    Other Parts Discussed in Thread: C2000WARE

    在使用C2000Ware_5_04_00_00\libraries\flash_api\f2803x中例程时,运行到

    // Verify the values programmed. The Program step itself does a verify
    // as it goes. This verify is a 2nd verification that…

  • TMS320F280039: 请问下能提供一份PMBus协议的Specification吗?

    Part Number: TMS320F280039
    Other Parts Discussed in Thread: C2000WARE

    TI专家您好!

    我在以下链接看到你们的一篇关于PMBus协议的Application Note:

    Software Implementation of PMBus over I2C for TMS320F2803x

    中提到了Part II of the Power Management Bus Specification,目前在做基于TMS320F280039的服务器数字电源…

  • TMS320F28P550SJ: Failed using tool ”serial_flash_programmer“

    Part Number: TMS320F28P550SJ
    Other Parts Discussed in Thread: C2000WARE

    我想要基于SCI进行串行编程,这样用户可以快速验证而不需要XDS下载器。

    然后我找到了一篇指导如何使用 “serial_flash_programmer” 进行SCI串行编程的文章:Serial Flash Programming of C2000 Microcontrollers (Rev. H)

    按照文章的说明,我将路径下:D:\TI…

  • TMS320F28379D: 如何在28379D实现biss-c通信

    Part Number: TMS320F28379D
    Other Parts Discussed in Thread: BOOSTXL-POSMGR, LAUNCHXL-F28379D, C2000WARE, CONTROLSUITE

    想在28379D实现biss-c,已经购买了BOOSTXL-POSMGR和launchxl-F28379D,但是没有配套开发板的28379biss例程,在c2000ware moter control sdk中关于biss的只有F28P65X的例程,请问是否提供LAUNCHXL…

  • TMS320F28335: CCS20.1.1如何创建新工程

    Part Number: TMS320F28335
    Other Parts Discussed in Thread: C2000WARE

    创建新工程的时候我的选择很少,就这些

    点击create,则会出现这个报错:Import failed for project '28335_IQsampleC' because its meta-data cannot be interpreted - please contact support。

    同时左上角出现标黄的文件夹

    我的c2000…

  • TMS320F28377D: 你好,请问TI有28377D CAN FIFO的例程吗?我在C2000Ware里面没有找到呀

    Part Number: TMS320F28377D
    Other Parts Discussed in Thread: C2000WARE

    如题,TI有28377D CAN FIFO的例程吗?我在C2000Ware里面没有找到呀

  • TMS320F28P650SH: 在芯片上跑Ucos RTOS内核,出现数据异常,由于P650的FPU是双精度 64位,之前用的都是单精度32位FPU,TI是否有对应的demo参考

    Part Number: TMS320F28P650SH
    Other Parts Discussed in Thread: TMS320F28388D, C2000WARE

    在芯片上跑Ucos RTOS内核,出现数据异常,由于P650的FPU是双精度 64位,之前用的都是单精度32位FPU,TI是否有对应的demo参考 ;

    查看资料,TMS320F28388D的FPU也是采样64位。

  • TMS320F280039C: dsp死机,看门狗没有正常复位,模块也没有进入NMI和非法中断,故障后晶振不起振

    Part Number: TMS320F280039C
    Other Parts Discussed in Thread: C2000WARE

    F280039C 模块正常拷机时,模块异常关机,can通信丢失并且不再恢复通信的问题,GPIO23被置高,必须重新上电才可以。
    watchdog是使能的,模块也没有进入NMI中断或非法中断,重新下电再上电后,模块恢复正常。
    刚开始用的是内部晶振2,开始怀疑是晶振异常,后为了方便进一步定位故障,改为了外部无源晶振,故障仍然可以复现,此时3.3V是正常的
    复现后,外部无源晶振无输出…

  • LAUNCHXL-F2800137: LAUNCHXL-F2800137开发板导入工程异常

    Part Number: LAUNCHXL-F2800137
    Other Parts Discussed in Thread: C2000WARE

    根据开发文档:/F280013xSeriesLaunchPadDevelopmentKit.pdf,安装CCS和C2000Ware_5_04_00_00后导入LAUNCHXL-F2800137工程异常。

    具体情况如下:

    1、打开C:\ti\c2000\C2000Ware_5_04_00_00\driverlib\f280013x\examples,可…

  • TMS320F280049C: 在CLA中调用sin/cos/sqrtf函数,程序会异常

    Part Number: TMS320F280049C
    Other Parts Discussed in Thread: C2000WARE

    在CLA中调用sin/cos/sqrtf函数,程序会异常

    请问该如何解决?

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong Daw Romanian
    Chinese Simplified Hungar…
  • LAUNCHXL-F28379D: 关于控制板时钟的一些疑问

    Part Number: LAUNCHXL-F28379D
    Other Parts Discussed in Thread: C2000WARE

    ti的工程师们你们好!

    我想请问一下就是launchxl-f28379d这块板子的cpu_timer能否自己调用开启计时或者关闭计时呢?比如我代码中某个变量通过if语句判断小于某个值就直接开启其中的一个cpu_timer进行计时(只进行计时(一直增大)做时间显示用,不产生中断信号且不设置周期)

  • TMS320F280039C-Q1: FLASH存储不进去,但是不报错

    Part Number: TMS320F280039C-Q1
    Other Parts Discussed in Thread: C2000WARE

    调用Fapi_issueProgrammingCommand(),不报错,但是数据没有存储进去,之后Fapi_getFsmStatus(),报0x30错误,但是flash区域我看过全是0xffff,没有数据

    用Fapi_doBlankCheck()函数也校验过这片区域全是0xffff,不应该写入不进去

    #ifdef __cplusplus
    #pragma…

  • LAUNCHXL-F28P55X: SCI_ex1加入EPWM失敗

    Part Number: LAUNCHXL-F28P55X
    Other Parts Discussed in Thread: SYSCONFIG, C2000WARE

    我在使用SCI的EX!後,想加入一個EPWM在PWM2A,也已經將設定調整至與成功過的專案一樣,但無法成功,以下是程式.c以及board.c

    //###########################################################################
    //
    // FILE: sci_ex1_loopback…

  • LAUNCHXL-F280039C: Program Download Failure

    Part Number: LAUNCHXL-F280039C
    Other Parts Discussed in Thread: C2000WARE

    Program Download Failure 程序下载失败 程序下载失败 程序下载失败 程序下载失败

    Symptoms: 症状:

    1. After DSP power-on: DSP上电后:

      • LED2 remains offLED2 保持熄灭(通常应闪烁或保持亮起)
      • LED3 stays constantly lit

  • TMS320F28388D: 使用Flash API 擦写时,是否需要解锁flash,进行擦写

    Part Number: TMS320F28388D
    Other Parts Discussed in Thread: C2000WARE

    看到st32操作flash擦写,需要先解锁flash,再进行擦写,然后再锁定(如下图)
    而在28388中只看到有关控制权(pump)的锁定(函数Flash_claimPumpSemaphore)和解锁(Flash_releasePumpSemaphore),没有看到关于flash的解锁与上锁,是否需要这个操作?

    TRANSLATE with x
    Eng…
  • TMS320F28384D: 芯片有两个C28x,是可以同时运行吗?

    Part Number: TMS320F28384D
    Other Parts Discussed in Thread: C2000WARE

    1、如下图,芯片有两个C28x,是可以同时运行吗? 

    2、有两个C28x同时运行的例程吗?

    3、CLA的运行频率和C28X的频率一样吗?

  • TMS320F280025C: 导入示例项目可以使用SysCtl_delay(),但如果自行引用sysctl.h来使用SysCtl_delay()就显示No source available for "SysCtl_delay()"

    Part Number: TMS320F280025C
    Other Parts Discussed in Thread: C2000WARE

    您好:

    我正在初学使用TMS320F280025C芯片,从C:\ti\c2000\C2000Ware_5_04_00_00\driverlib\f28002x\examples\led导入这个LED闪烁的项目时,main函数中的Device_init();跳转→SysCtl_setClock(DEVICE_SETCLOCK_CFG);跳转→…

  • TMS320F2800157: ADC例程异常

    Part Number: TMS320F2800157
    Other Parts Discussed in Thread: C2000WARE, TMDSEMU200-U

    你好,我尝试了adc例程ex1,ex10,ex11,ex2,ex4等等,出现了如图报错

  • TMS320F280025C: F280025C是否支持InstaSPIN-FOC和FAST

    Part Number: TMS320F280025C
    Other Parts Discussed in Thread: C2000WARE-MOTORCONTROL-SDK, C2000WARE

    请问F280025C是否支持InstaSPIN-FOC和FAST?

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong Daw Romanian
    Chinese…
  • C2000WARE: download Access denied

    Part Number: C2000WARE

    when i try to download Windows Installer for C2000Ware,will show me 

    Access denied

    We are unable to approve your download at this time.

     If you feel you have been denied incorrectly, please contact the TI Customer Support Center…
  • TMS320F280049C: VCU0与eabi格式、coff格式支持的问题

    Part Number: TMS320F280049C
    Other Parts Discussed in Thread: C2000WARE

    TI的工程师你们好!我现在在利用C2000ware中(版本:5.4.0)的VCU部分进行官方FFT的移植。280049C的VCU类型是VCU0/1,因此应当加入c28x_vcu0_library_fpu32.lib,并加入vcu0_types.h,vcu0_fft.h,我发现在COFF格式下对VCU文件夹2837xFFT例程的移植是成功的,无报错,但是若调整为eabi格式…

1 2 3 4 5 »