• TMS320F28335:28335的烧录问题

    Part Number: TMS320F28335

    为什么芯片下载不了程序,这是为什么?
    C28xx:连接到目标时出错:(错误 -230 @ 0x0)JTAG IR 和 DR 扫描路径的测量长度无效。这表示 link-delay 或 scan-path 中存在错误。(仿真包 9.5.0.00143)

  • TMS320F28035: 发波异常

    Part Number: TMS320F28035

    想做个PWM1A、2A、3A同步计数,然后2A、3A相对于1A同时改变占空比与位移的程序,结果发现 经常会出现占空比出错的问题,某个pwm会随机发出100%占空比的输出一个周期,下个周期才能正常,有办法解决嘛。相位与占空比都限制了上限,不会超过80%占空比。

  • TMS320F280025: 在配置使用其CAN的BUSOFF测试时,针对ACK位的干扰BUSOFF功能正常,但在针对RTR位的干扰时候,无法进入BUSOFF的状态,导致BUSOFF逻辑失效

    Part Number: TMS320F280025

    如上是bus_off测试结果;如下是底层配置代码:

    //初始化配置

    GPIO_setPinConfig(GPIO_30_CANA_RX);
    GPIO_setPinConfig(GPIO_31_CANA_TX);
    //初始化CAN模块
    CAN_initModule(CANA_BASE);
    //设置波特率
    // CAN_setBitRate(CANA_BASE, DEVICE_SYSCLK_FREQ, 500000, 20);
    CanaRegs…

  • TMS320F28035: 尝试把用汇编语言编写的中断函数封装成.lib库过程中,编译时出现structure/union tag can't be global的提示错误/During the process of attempting to encapsulate interrupt functions written in assembly language into the. lib library, an error message stating 'structure/union

    Part Number: TMS320F28035

    使用CCS3.3进行函数封装,在编译时出现错误的类型和相应的structure和union详情如图所示。在有同样的头文件情况下,封装另一个C语言编写的函数代码可以封装成.lib文件。出现这种错误该如何解决/

    In CCS 3.3.The types that encountered errors during compilation and the corresponding structure and union details are shown…

  • TMS320F28035: CLAsin,在将程序正常烧写到flash中时,返回值正常。但是通过串口升级方式将程序烧进去后CLAsin与CLAcos返回值不正常。但是CLAdiv,CLAsqrt是正常的。

    Part Number: TMS320F28035
    Other Parts Discussed in Thread: UNIFLASH, C2000WARE

       。bootload中只是执行了一条跳转指令而已。为什么什么导致CLAsin,CLAcos不正常。而其他CLA math函数是正常的。如果不用bootlad升级,直接将应用程序烧进去就全是正常的。

  • TMS320F28035: FLASH maximum erase time

    Part Number: TMS320F28035

    As shown in the figure, the typical value of the erasure time for a single 8k sector of the TMS320F28035 is 2 seconds, and the maximum value is 12 seconds.

    Now,There are two questions.

    1. What is the approximate proportion…

  • TMS320F28035: 在程序中的结构体定义中直接初始化变量有警告提示使用C++11但在编译器中无法更改C++03为C++11

    Part Number: TMS320F28035
    Other Parts Discussed in Thread: C2000WARE

    struct CANMBOXn_DATA { union CANMSMID u32MID; Uint16 Dlc = 8; union CANMDR unMDR; };

    仿真查看

    仿真时可以看到在 结构体定义初始化为7的时候不初始化定义的结构体 Dlc的值默认是7

    在实际工程中直接使用会有问题么?

  • TMS320F28035: 烧程序报错 Error connecting to the target:

    Part Number: TMS320F28035

    C28xx: Error connecting to the target: (Error -1015 @ 0x0) Device is not responding to the request. Device may be locked, or the debug probe connection may be unreliable. Unlock the device if 烧程序报错 jian'chapossible (e.g. use…

  • TMS320F28035: TI工具 SFRA使用的几个疑问

    Part Number: TMS320F28035
    Other Parts Discussed in Thread: SFRA

    1。 SFRA中用的ref,fdbk, out都是归一化的嘛。也就是我的采样,参考,环路计算结果都要处理成0~1范围内的值才能使用?

    2。 SFRA必须配合TI 提供的算法库使用嘛?配合自己的算法,行不行?

    3.   SFRA必须使用串口嘛?

        我当前板子没有串口,因此我使用了CAN转串口工具进行了协议转换。查看数据,GUI发送的数据都有及时回复,但是GUI还是有重发。并且实际使用效果看…

  • TMS320F28035: DSP 程序在进入用户main函数之前会有初始化吗

    Part Number: TMS320F28035

    如题,DSP在上电进入用户main函数之前,会有初始化GPIO端口电平操作吗?我现在一个电路板上控制了一组LED,这些LED通过开漏控制,低电平熄灭LED,高电平或悬空时,点亮LED。

    实际测试时,发现我有某个LED灯错误点亮,多次上下电测试,每次这个GPIO都会被错误点亮,其余GPIO则没有这个问题。

    我用仿真器调试时,也发现在仿真器即将进入main函数时,这个灯就被点亮,但其余GPIO都没被错误点亮。我想知道这是什么原因?我这一组LED的电路及参数都一样…

  • TMS320F28035: 可以在035添加mbedtls库是否可行

    Part Number: TMS320F28035
    Other Parts Discussed in Thread: C2000WARE,
    • 1可以在035上添加mbedtls 实现对一些加密算法的快捷操作吗?
    • 2如果不能调用mbedtls库,可否使用c2000ware中的libraries\security\crypto\c28中的aes和sha加密算法在035上实现aes的加解密以及HMAC-SHA 256对密钥的组合
  • TMS320F28035: 作为I2C从机的延时响应

    Part Number: TMS320F28035

    用DSP28035的I2C设备作为从机,与上位机(主机)通信;当接收到上位机指令时,DSP作为I2C从机需要向上位机发送响应数据,现在遇到的问题是:

    当DSP从机接收到上位机指令后,需要延时10S左右,再向上机发送响应数据,如果直接延时,会导致数据无法发出,有什么解决方法?谢谢!

  • TMS320F28035: CLA程序为何编译出大量的空指令

    Part Number: TMS320F28035

    err = fabs(ClaLoop->err); 00009196: 73E10000 MMOV32 MR2, *MAR0, UNCF 00009198: 7E20000A MABSF32 MR2, MR2 0000919a: 74E08CD0 MMOV32 @0x8cd0, MR2 0000919c: 7FA00000 MNOP 0000919e: …

  • TMS320F28035: Using the function in CLAmath compiles with a warning “Data is being written to auto-generated file 28035 NIMI CLA.i10”

    Part Number: TMS320F28035
    Other Parts Discussed in Thread: CONTROLSUITE

    I added the .lib file “ cla0 math library.lib” and the .h file “CLAmath” to the project. Both files are found in “D:\CONTROLSUITE\controlSUITE\libs\math\CLAmath\v4_02_00_00” and I…

  • TMS320F28335: 无法创建工程(Cannot create CCS project)

    Part Number: TMS320F28335

    (Cannot create C2000 type of CCS project)无法创建C2000类型的工程

  • TMS320F28035: 没办法找到XDS100

    Part Number: TMS320F28035

     一直出现这样的问题,在文件夹里面也没找到XDS100的有效安装程序

  • TMS320F28034: Flash烧录程序断电,再次上电程序未保存。

    Part Number: TMS320F28034

    我用CCS12.8打开了一个CCS3.3版本的程序,并将编译器版本修改为TI v6.4.12,BIOS版本修改为5.42.2.10,之后成功编译生成了.out文件,将.out文件烧录进FLASH后程序正常工作(程序中有关于LED屏幕显示的内容,我通过LED是否正常工作来判断程序是否烧录成功),之后断电重启LED不亮了,程序未被保存。想请问下是什么原因。

    我在lib中添加了SFO_TI_Build_V6还是不行,断电后程序消失。

    下面我粘贴一下MEMORY与SECTIONS的代码…

  • TMS320F28035: Flash_Verify(Flash_ptr,Buffer,Length,&FlashStatus);操作失败

    Part Number: TMS320F28035
    Other Parts Discussed in Thread: C2000WARE

    在使用C2000Ware_5_04_00_00\libraries\flash_api\f2803x中例程时,运行到

    // Verify the values programmed. The Program step itself does a verify
    // as it goes. This verify is a 2nd verification that…

  • TMS320F28035: ADC初始化和EPWM冲突

    Part Number: TMS320F28035

    在使用EPwm中断的程序中,我将ADC初始化InitAdc()函数放在EPWM模块的TBCLK(时基时钟)关闭和开启前,AdcResult全为0,如果放在TBCLK(时基时钟)关闭和开启后,AdcResult就有值。

    想请问下这是什么问题。

    TRANSLATE with x
    English
    Arabic Hebrew Polish Bulgarian Hindi Portuguese Catalan Hmong …
  • TMS320F28035: 串口下载报错

    Part Number: TMS320F28035

     请问串口下载显示这个错误是什么问题

  • TMS320F28035: bootloader 将bin文件写入flash,跳转APP失败

    Part Number: TMS320F28035

    我用bootloader接收完程序后,进入跳转APP始地址后,bootloader程序会复位,重新进入引导程序,这是为什么?这是我CMD文件编写有问题吗?始地址为0x3e8100; APP的begin 为0x3e8100

  • TMS320F28035: CCS10.1.1.00004仿真时会断开

    Part Number: TMS320F28035
    Other Parts Discussed in Thread: TMS320F28069,

    已经仿真运行,且Expressions窗口也能实时刷新变量,运行一段时间后未做任何操作,就断开了.

    仿真器100v3, TMS320F28069/TMS320F28035都遇到同样的问题。

  • TMS320F28035: 峰值电流模式控制,如何配置产生PWM1A与PWM1B互补

    Part Number: TMS320F28035

    请问峰值电流控制模式,如何产生互补PWM,峰值控制模式时,PWM是由TZ模块的CBC功能关断的,但是TZ在DB模块之后,无法生成互补PWM了,那同步整流的BUCK该如何驱动。是不是F28035不可以,但是F280025可以。

  • TMS320F28035: lin接收id为0x3c的帧

    Part Number: TMS320F28035

    使用TMS320F28035的LIN做从机接收id为0x3c的帧不能进入接收中断。但是在loopback模式或外部引脚连接自发自收时能够进入接收中断。是LIN不能接收到id为0x3c的帧吗

  • TMS320F28035: Flash_Program函数写入问题。

    Part Number: TMS320F28035
    Other Parts Discussed in Thread: C2000WARE

    在copy函数中调用库函数Flash_Program,数据无法写进flash。

    资料说是要在RAM执行。使用了以下两种方式都不行。

    1,#pragma CODE_SECTION(copy, "ramfuncs");

    2,#pragma CODE_SECTION(Flash_Program, "ramfuncs");这种会警告Flash_Program没定义…

1 2 3 4 5 »