TPA3255是否可以AB通道输入的音频信号由AB输出通道输出,CD通道输入的音频信号由CD输出通道输出。即两路互不影响,可独立使用。
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplified | Hungarian | Russian |
Chinese… |
TPA3255是否可以AB通道输入的音频信号由AB输出通道输出,CD通道输入的音频信号由CD输出通道输出。即两路互不影响,可独立使用。
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplified | Hungarian | Russian |
Chinese… |
TPA3255如何实现闭环反馈?根据TPA324x and TPA325x Post-Filter Feedback文档画好PCB,电路无法正常工作(PWM振荡一下就停止了),把反馈回路断开就能正常工作。有哪些地方需要注意?有没有关于反馈回路更详细的设计参考?
Hi ti team,
使用AP测试 TPA3255EVM,发现TPA3255RVM会出现保护。请帮忙分下原因
测试条件:
1,AP输入信号800mV;输入频率100HZ;对AP输入信号不断的打开和关断,TPS3255会出现保护。如附件视频
2,功率120W,4R负载,PVDD=51V。
请问TPA3255的PVDD_AB和PVDD_CD,在BTL模式下,能否单独供电?比如我只用AB通道构建一个BTL,那么想不给PVDD_CD供电,以减少干扰,降低噪声等。
用TPA3255做了一块功放板,采用的PBTL模式,频率600K。
电源用AC转DC供电(AC220V转DC51V),功放运行正常,输出接4欧姆负载,200W,接散热片,1K正弦波可持续运行5分钟。
电源换成DC转DC(DC24V转DC52V),其他不变,1K正弦波运行约3秒,就直接过热保护。电源输出功率无异常,接电子负载可输出400W。
电源纹波对比,AC转DC的电源…
你好,有没有70V、100V定压功放方案推荐?目前需求是100W;
我计划用TPA3255做一款汽车功放.
但目前遇到一个问题, 当播放过程中出现故障的时候, TPA3255需要手动按下按键,才能停止工作\重启工作, 否则扬声器会继续发出鸣响(TPA3255无法初始化的时候.)
这对于汽车音响来说无疑是无法接受的.
请问以下ti的工程师们, 在不需要软控和手动控制的情况下, 有没有办法让它初始化
参考EVM评估板设计的功放板,PBTL模式下,输入信号到达削波电压后出现不正常的削波警告和工作现象。
削波警告指示灯不是一直常亮而是很快频率的闪烁,芯片输出的波形里面也是同频率的输出中断。
电感出现滋滋的声音。
在查看TI TP3255 demo图纸时,有些疑问需要咨询:
若给评估板使用48V 10A的电源供电。
原理图如slar129a.pdf
1:RCA input 输入单端信号幅值范围是多少?输入差分信号幅值范围是多少?
2:RCA输入与功放输出之间的关系是什么?
3:RCA输入信号幅值多少,可以使得输出功率最大300w?
4:在功放需要300w输出时,评估板的电源有什么要求?只需要大于功放输出功率再预留些预留就可以,
还是需要与功放的容抗参数需要协调…
Hi Team,
The PVDD is 24V and the GVDD is 12V in my application, the attachment is my schematic.one heat sink is attached on the TPA3255.
When the reset signal is low and the actually voltage of the 24V power rail is about 12V(the input…
你好:
想问下TPA3255-Q1按照PBTL方式设计。未安装散热片的情况下。也未让音频功放输出,温度也很高会触发保护,这样正常吗?还是有哪些因素造成了影响?
Hi
客户再使用TPA3255 时,用两颗做2.1应用,发现再无音源信号输入时,不接负载的情况下芯片会发烫,接通电源10分钟左右温度会去到70~80°左右。如下是线路图,还请帮忙分析。谢谢
FS-T889_Stereo50W+250W_(BP1048B2+TPA3255x2+JW5121)_20230907.pdf
Hi Team,
I looked at the ticket:https://e2e.ti.com/support/audio-group/audio/f/audio-forum/974598/tpa3255-using-tpa3255-to-drive-a-transformer-in-btl-and-pbtl-config. it mentioned a document which involved the transformer content…
供电电压48V,使用TPA3255 SE 4.0模式,当输入20Hz至40Hz正弦波信号,每通道负载4欧@5W时,电源电压会由48V升高到60至70V之间. 而且当加大输出功率超过20W@4欧@35Hz时芯片会保护.
这种问题和什么有关?应该怎么解决?
Hi team,
Would you please share some documents about the LC+transformer configuration? I`m debugging the TPA3255+LC+transformer. the problem I met is that the voltage is not continue to rise during rising the input voltage of TPA3255…