Other Parts Discussed in Thread: LMX2572
请问LMX2594设置从1GHZ扫到1.5GHZ,步进1MHZ,10秒扫完,扫描6个周期,每个地方要如何选择,怎么设置,怎么计算,有没有相应的指南,谢谢!
你好:
我在使用LMX2594时,参考频率选择为100MHz,使能OSCin 倍频器,Fpd=200MHz,选择VCO4=12GHz,仅使能OUTPUT A,分频器配置为4,输出3GHz,框图如下;
频谱仪测试3GHz输出,发现750MHz杂散,结果如下所示,通过寄存器R0,设置成0x2519,power downLMX2594时杂散消失;
mx2594的配置如下:
地址 值
0x00 251A 复位寄存器,10ms后取消复位
0x00 2518
0x4E…
请教LMX2594使用方法,输入156.25Mhz,输出2个5GHz时钟给ADC12DJ5200使用,帮忙看下原理图是否有问题,TICS pro生成的工程文件对吗?
在配置2594全辅助校准模式下,读回读寄存器完全不正确,R110,R111,R112以及专用的回读寄存器R107,R108,R109也不正确,但是读我写入的寄存器是正确无误的;R0为2418
请查看以下连接问题,之前和TI专家讨论问题并没有得到解决
在配置2594全辅助校准模式下,读回读寄存器完全不正确,R110,R111,R112以及专用的回读寄存器R107,R108,R109也不正确,但是读我写入的寄存器是正确无误的;R0为2418,有什么地方是需要配置的吗
LMX2594输出任意频点都会在左右出现等间距干扰信号,怎样去除?
各位TI专家,我在看这个文档:
TIDA-01410 (tidud11.pdf)
Phase Synchronization of Multiple PLL Synthesizers Reference Design
第2.2.1节“相位同步理论”中,有这样一段话:
For instance, whenever a signal is…
hi,I want to know harmonic requirements of the reference clock。When the harmonic is better than any index, the PLL output spurious is not affected by the clock power.
LMX2594修改输出功率寄存器R44,从0-63,频谱有异常杂散,视频中配置的是2G 频率,已锁定后,再修改R44寄存器,寄存器配置如下
我用2594生成了一个2.64GHz信号,但是二次谐波及以上谐波均未达到手册中的谐波抑制度,也试着调整未使用的差分输出焊盘,均没有改善,想请教一下各位如何能做到较好的谐波抑制。