• AMC1200: AMC1200

    Part Number: AMC1200

    AMC1200的输出如果短路到+5.7V,会不会造成器件损坏?

  • INA240: INA240使用不对称正负电源

    Part Number: INA240
    Other Parts Discussed in Thread: ISO124, AMC1200, AMC1301

    如果使用+3V-1.6V给   运放供电,不平衡正负电源是否对运放使用性能造成什么影响,假设我对于一些宽电源供电的运放使用+24V-5V不平衡运放情况是否又和这种窄供电电源运放情况类似

  • AMC1200: AMC1200采样50KHZ模拟信号问题

    Part Number: AMC1200
    Other Parts Discussed in Thread: AMC1350, AMC1351

    需要对50KHZ,高2.6V,低0V的方波模拟信号进行隔离采样,考虑使用AMC1200芯片是否合适,因为我看手册其带宽只有100KHZ不对我模拟信号大多少,而且该芯片上升下降时间也达到us级压摆率很低估计不能很好跟踪到输入高频方波信号。

  • AMC1200: 这边想用TI的AMC1200BDWV这款芯片,麻烦帮忙问下技术支持,这个新品的单端输入电压是需要2k并联28K电阻后再去分压计算吗?

    Part Number: AMC1200

    Hi TI TEAM,

    这边想用TI的AMC1200BDWV这款芯片,麻烦帮忙问下技术支持,这个新品的单端输入电压是需要2k并联28K电阻后再去分压计算吗?

  • THS4531: 直流输入时输出产生20MHz纹波问题

    Part Number: THS4531
    Other Parts Discussed in Thread: AMC1200,

    尊敬的TI专家们:

    为了驱动28377的16位ADC,我使用了若干如下电路进行单端转差分操作。共有5个通道,其中两个SMA输入,两个AMC1200隔离运放输入,一个取自本地的3V基准经过分压和缓冲后输入。

    调试时发现,两个SMA输入的单端转差分电路中的一个,无论sma接口是开路、短路、连接信号发生器输出直流电压,差分输出总是会有一个约20M、20mVp-p的交流成分。差分输出的…

  • AMC1200: amc1200问题,放大倍数不是恒定的8倍

    Part Number: AMC1200

    如下图,

    当输入是0.16v,输出是1.91v,放大倍数是11.93倍

    当输入是0.08v,输出是1.6v,放大倍数是20倍

    当输入是0.032v,输出是1.4v,放大倍数是43.75倍

    请问这是什么原因?

  • AMC1200: 输出电压问题。

    Part Number: AMC1200

    AMC1200B在原边VDD1未供电,副边VDD2供电的情况下,VOUTP和VOUTN之间的电压是多少。

  • AMC1200: TI AMC1200的使用疑问

    Part Number: AMC1200

    我的电路图如下,使用AMC1200获取R11两端的电压差,我上电后,J13未接负载,我的R9电阻就冒烟了。

        是不是我这个使用方法不对?有推荐的电路?这个电路是用来采集汽车交流充电桩上的CP信号电压值?

  • AMC1200: AMC1200差分信号增益倍数偏大问题

    Part Number: AMC1200
    Other Parts Discussed in Thread: ADS1115,

    FAE你好:

    请看下面的电路图,这个是电压绝缘检测电路,分压电阻都是 0.1%的,根据计算可以 DC=750v,两个分压电阻的上的电压是121.3mv左右,

    实测P+/-和 N+/-的差分电压:115.5mv,115.5mv(mv及万用表测试)

    增益后的差分电压ISOP+/-和ISON+/-电压:989mv,987mv,增益后的信号直接接入ADS1115,

    按照8倍计算的话…

  • AMC1200: 断电瞬间,输出端会产生脉冲,如何消除?

    Part Number: AMC1200

    您好,

      我是用AMC1200做电流检测,VDD1 VDD2都由外部24V转换而来,其中VDD2由VDD1隔离而来。在断掉24V瞬间,AMC1200的输出会有一个12ms左右的脉冲,影响后端电路,请问有办法消除这个干扰吗?

    以下是电路图:

    黄色信号:电流

    蓝色信号:输出电压波形

    黄色波形:电流

    蓝色:VDD1

    粉色:VDD2

  • 请教芯片(隔离差分运放,放大倍数为1或者可调,精度达到0.1%)

    Other Parts Discussed in Thread: AMC1200, ISO124

    请教各位能否推荐隔离差分运放,精度能够达到0.1%的,AMC1200精度不是很高,谢谢。

  • AMC1200芯片

    Other Parts Discussed in Thread: AMC1200

     请问前辈,我用的TI芯片:AMC1200BDUBR 在工作时引入了112MHz和132MHz的EMC 噪声。请问电路要怎么改进才能消除这个噪声?望前辈能帮忙推荐解决方法 不胜感激!

  • 请教AMC1200应用问题

    Other Parts Discussed in Thread: AMC1200, AMC1301

     

    使用AMC1200隔离放大器作为电压采样,电压通过分压电阻,分到-250mv~+250mv之间。

    采样输出V1++是接到AD采样端口。下图中,VCC1为5V,VCCA为5V,-VCCA为-5V。

    1.当VIN+,VIN-接上输入电压时,经过AMC1200隔离放大,再通过运放输出,此时AD采样的值会波动30个采样点左右(12位AD,最大4095)。

    2.当VIN+,VIN-接上输入电压时,不经过AMC1200隔离放大…

  • 关于AMC1200前端电阻分压问题

    Other Parts Discussed in Thread: AMC1200

    请问AMC1200前端可以采用以下电路吗,我只要保证R155两端的分压为小于±250mv,应该就可以了吧。

    不管我外面接的是100V或者值1000V。主要是我看很多都是将采样电阻放在了最底端(R25位置)。

  • 关于AMC1200差分输出问题

    Other Parts Discussed in Thread: AMC1200, AMC1301

    采用AMC1200进行电流采样,如图片当VDD1和GND1没有供电,VDD2和GND25V供电时,VOUTP和VOUTN输出差值为2.5V左右?这是为什么呢?

  • 模拟量隔离

    Other Parts Discussed in Thread: AMC1200, ISO124

    大家好,想用AMC1200隔离0~5V的电压,但看到输入是±250mv,增益为8,输出最大才是2V吗?

  • AMC1200输入电压

    Other Parts Discussed in Thread: AMC1200想用AMC1200隔离0~5V模拟量,但手册前面写的输入电压是GND1-0.5~VDD1+0.5,后面又写的是±250mv,怎么回事?能隔离0~5V电压吗?
  • amc1200是否可以应用在采集4-20mA电流采集

    Other Parts Discussed in Thread: AMC1200

    请问amc1200是否可以应用在采集4-20mA电流采集,具体采集电路要怎么处理

  • 关于AMC1200在电机驱动电路中使用的疑惑

    Other Parts Discussed in Thread: AMC1200

    我用三菱的IPM PS21964做电机控制,用三片AMC1200分别做两相电流采样和母线电压采样。下图是官方手册的典型应用接线图。

    因为把1200的GND1(4脚)误接到IPM的地(相当于接到了上图中的HV-)导致1200烧坏。但若按照上图的接法,我想了解图中的浮空电源输入(Floating Power Supply)是怎么工作的?因为15V并不是相对于GND1的15V而是相对于HV-的15V。而且它又该接到哪里去呢…

  • AMC1200的差分输出与DSP芯片ADC接口怎么连接

    Other Parts Discussed in Thread: AMC1200

    各位大大们你们好,我看到AMC1200的数据手册,差分输出两路信号中间并联了滤波电阻,然后直接就接到了DSP的ADC采样接口。我比较疑惑是因为DSP的ADC接口可以设置为差分信号采样模式吗? 这个连接的方式什么原理呢?

  • AMC1200使用单端工作方式

    Other Parts Discussed in Thread: AMC1200

    想用AMC1200采集外部送入的模拟量,输出量送给单片机的AD口,AMC1200采用单端工作模式可以?看到的资料用的都是工模输入

  • AMC1200B做电流检测时输入端电压

    Other Parts Discussed in Thread: AMC1200, AMC1100

    想用AMC1200做24V或者48V的电池放电电流检测。

    查看AMC1200的手册,提示输入端的共模电压Vcm 只有5V,请问按照附件的原理图设计是否正确,若错误,该如何修改?

  • AMC1200可以测量直流电压和直流电流吗?

    Other Parts Discussed in Thread: AMC1200, OPA2188, OPA2171

    AMC1200可以测量直流电压和直流电流吗?

  • 隔离放大器的选择

    Other Parts Discussed in Thread: AMC1200

    1、输入电压:0V--32V

    2、输入阻抗:>=300k

    能不能推荐一款隔离放大器。

    如果使用AMC1200,后端ADC为单端输入,AMC1200的输出负该怎么处理?可以直接悬空么?

  • AMC1200、AMC1301隔离运放咨询

    Other Parts Discussed in Thread: AMC1200

    用此隔离运放采集400V左右电压,前端用电阻将分压到输入口为合适电压范围,隔离运放为差分输出。后面不想再加一级运放,这样既增加成本又损失精度。输出差分电压可不可以用单片机的两个AD口直接采集。采样结果相减。datasheet首页里的图描述为供电电压为3.3V时,差分电压以1.29V为基准,这样理解不知道是否有误。

1 2 3 4 5 »