• TMS320F28377D: C2000-28377D-adc&cmpss - 差分信号与cmpss相匹配的问题?

    Part Number: TMS320F28377D
    如果我现在使用的差分信号的模式进行电流采样,同时我还想使用cmpss功能,
    我想问一下是否需要将差分信号每一路叠加一个ref,即叠加一个直流量在cmpss能够比较合理的范围内?

    其次从cmpss原理框图上来说,使用的是CMPINxP,这个管脚才是比较输出对象,
    CMPINxN这个管脚只是比较参考其中的一个选择而已?
    即:如果要比较必须要接入CMPINxP才可以,并且电平必须叠加一个直流分量吗?



  • TMS320F28P550SJ: Failed using tool ”serial_flash_programmer“

    Part Number: TMS320F28P550SJ
    Other Parts Discussed in Thread: C2000WARE

    我想要基于SCI进行串行编程,这样用户可以快速验证而不需要XDS下载器。

    然后我找到了一篇指导如何使用 “serial_flash_programmer” 进行SCI串行编程的文章:Serial Flash Programming of C2000 Microcontrollers (Rev. H)

    按照文章的说明,我将路径下:D:\TI…

  • TMS320F28P650SH: 在芯片上跑Ucos RTOS内核,出现数据异常,由于P650的FPU是双精度 64位,之前用的都是单精度32位FPU,TI是否有对应的demo参考

    Part Number: TMS320F28P650SH
    Other Parts Discussed in Thread: TMS320F28388D, C2000WARE

    在芯片上跑Ucos RTOS内核,出现数据异常,由于P650的FPU是双精度 64位,之前用的都是单精度32位FPU,TI是否有对应的demo参考 ;

    查看资料,TMS320F28388D的FPU也是采样64位。

  • TMS320F280025C: 导入示例项目可以使用SysCtl_delay(),但如果自行引用sysctl.h来使用SysCtl_delay()就显示No source available for "SysCtl_delay()"

    Part Number: TMS320F280025C
    Other Parts Discussed in Thread: C2000WARE

    您好:

    我正在初学使用TMS320F280025C芯片,从C:\ti\c2000\C2000Ware_5_04_00_00\driverlib\f28002x\examples\led导入这个LED闪烁的项目时,main函数中的Device_init();跳转→SysCtl_setClock(DEVICE_SETCLOCK_CFG);跳转→…

  • TMS320F28021: 求助:CCS4.2工程移植到12.5遇到的若干问题

    Part Number: TMS320F28021

    在将V4.2的工程移植到V12.5版本的CCS的过程中,遇到了一系列的配置以及编译的问题,个人能力有限,不知道应该如何解决,请求各位大佬的帮助,万分感谢!orz

    1首先,我的文件结构是正确的吗?我注意到F28021.cmd文件中提到需要在工程中添加bios.cmd,而我的文件中也确实有这个cmd文件。但是common 文件下已经有了一个F28021.cmd文件(原本工程就有的),header 文件下面也有了一个 bios.cmd文件(也是原本工程就有的…

  • TMS320F28P650DK: Is there any detail introduction,description or training technical documents about cyber security according to ISO21434 standard of TI C2000 MCU?

    Part Number: TMS320F28P650DK

    Dear TI Team:

             Is there any detail introduction,description or training technical documents about cyber security according to ISO21434 standard of TI C2000 MCU?Because Automotive industry will mandatory implement ISO21434…

  • TIDM-02009: Is there any detail introduction,description or training technical documents of software resolver decoding in TIDM-02009 design?

    Part Number: TIDM-02009

    Dear TI Team:

            Is there any detail introduction,description or training technical documents of software resolver decoding in TIDM-02009 design?I want to learn about the whole process of EPWM moudule and hardware electric circuit…

  • TIDM-02014: Is there any detail introduction,description or training technical documents of software resolver decoding in TIDM-02014 design

    Part Number: TIDM-02014
    Other Parts Discussed in Thread: TIDM-02009

    Dear TI Team:

            Is there any detail introduction,description or training technical documents of software resolver decoding in TIDM-02014 design?I want to learn about the whole process…

  • TIDM-02009: How can I get the TUV SUD Rail GmbH ASIL D technical report of TIDM-02009 Design

    Part Number: TIDM-02009

    Dear TI Team:

            How can I get the TUV SUD Rail GmbH ASIL D technical report of TIDM-02009 Design?I think it is  confidential, NDA agreement might need be signed with TI.We need this certificate files to convince our  OEM customer…

  • TIDM-02009: Where can I find the software project of the TIDM-02009 design?

    Part Number: TIDM-02009
    Other Parts Discussed in Thread: C2000WARE

    Dear TI Team:

             Where can I find the software project of the TIDM-02009 design?I have search the "C2000Ware_DigitalPower_SDK_5_04_00_00" and "C2000Ware_MotorControl_SDK_5_03_00_00",there…

  • C2000-GANG: 如何通过cJTAGD的2脚下载程序?

    Part Number: C2000-GANG

    公司产品预留的下载口是:TMS\TCK\3.3\GND,用CCS可以正常下载,但是产线生产较慢,现在用C2000-GANG下载,又报错,芯片用的是280039C,

    我搜了一下,论坛上说支持CJtag但是没有说具体的方法,

    [FAQ] TMS320F280039C: 更新了 C2000 GANG 以支持 TMS320F28003x 器件 - C2000Tm︎ 微控制器论坛 - C2000 微控制器 - E2ETm 设计支持

    [FAQ] [参考译文] [FAQ…

  • TMS320F28379D: 如何理解FSM状态机图

    Part Number: TMS320F28379D

    请问大家,在“使用C2000可配置逻辑块(CLB)进行设计”这篇文献中,FSM状态机图是怎么得出来的,S0和S1代表什么状态?谢谢

  • TMS320F28377D: CPU1控制eMIF1的CS3空间与 FPGA异步通讯,CPU2控制eMIF1的CS2空间与AD7616模拟采集芯片通讯,双核同时使用时数据有异常,单核CPU使用时正常

    Part Number: TMS320F28377D
    eMIF初始化函数如下,请帮忙指出问题,给出解决方案,谢谢!
        
    void InitEMIF(void)
    {
        EMIF_AsyncTimingParams tParamAsync;
        EMIF_SyncConfig sdConfig;
        EMIF_SyncTimingParams tParam;
        /********************************EMIF1 FOR FPGA*********************…
  • TMS320F280025C: 移植SYS/BIOS后 System_printf无法打印输出 且Task创建后过一会就卡死 是否有什么配置没完成的?有无官方移植成功的示例工程参考?

    Part Number: TMS320F280025C

    参考以下成功进行移植后 C代码如下:

    [【TI C2000】F28002x移植SYS/BIOS并运行TI-RTOS及工程模板](blog.csdn.net/.../145650628)

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    /*
    * ======== main.c ========
    */
    /* BIOS/XDC Include Files. */
    #include <xdc/std.h>
    #include <xdc/cfg/global.h>
    #include
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • TMS320F280025C: 非FIFO模式下 如何开启SCI中断?

    Part Number: TMS320F280025C

    代码如下 开启后调试无法进入中断函数 但在阻塞接收下测试接收没问题

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    /**
    * main.c
    */
    #include "device.h"
    #include "driverlib.h"
    #include <stdint.h>
    #include <stdlib.h>
    #include <stddef.h>
    #include <string.h>
    #include <stdio.h>
    #include <math.h…
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • TMS320F280025C: F280025C是否支持TI-RTOS?如果支持 如何在工程中移植?

    Part Number: TMS320F280025C
    Other Parts Discussed in Thread: SYSBIOS,

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    /**
    * main.c
    */
    #include "device.h"
    #include "driverlib.h"
    #include <stdint.h>
    #include <stdlib.h>
    #include <stddef.h>
    #include <string.h>
    #include <stdio.h>
    #include…
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • TMS320F280039: 求推荐一款做维也纳PFC的C2000系列型号推荐.

    Part Number: TMS320F280039

    1.最近公司要开发一款40KW左右的维也纳PFC,需要选型一款DSP;

    2.DSP主要做维也纳PFC控制,对外会输出一路RS485给到主控,主要是通讯启停和故障信息,其它功能不需要;

    3.比较久没模DSP了,之前用过28335,看了下市场上目前比较常用的型号有28335、28035、28034、2837X、28004X、28003X系列;

    4.个人想法是找一款成本相对比较低一些,能满足要求的型号,大概看了下28003x硬件外围电路也比较简单,这款是否合适…

  • TMS320F280049C: 数字电源开发问题请教及TIDA-010062参考项目LLC的控制策略

    Part Number: TMS320F280049C
    Other Parts Discussed in Thread: TIDA-010062

    各位TI的专家,你们好!

    最近我公司要开始做数字电源开发,想使用贵公司的C2000系列实时控制IC,现有以下问题要请教下:

    1、目前我们要开始的项目是以TIDA-010062为参考项目的无桥PFC+LLC,功率1.3KW左右,请问下你们的这个参考设计有客户使用过并且稳定运行吗?

    2、可否推荐几款常用的C2000数字电源控制IC,我们可能使用成本稍低些的…

  • TMS320F28379D: 關於ti c2000 gang 的jtag 定義

    Part Number: TMS320F28379D

    各位帥哥美女們早安,

    請問一下, ti c2000 gang  的Jtag 定義有嗎?

    原因是我們做了個硬體, 裡面的Jtag接了以下的腳位,可是我不知道要怎麼接到那二排的腳位上?

    7       GND
    6       MID_TRSTN
    5       MID_TDI
    4       MID_TCK
    3       MID_TMS
    2       MID_TDO
    1       VDD_3v3

    麻煩各位, 感謝!

  • TMS320F28377D: CPU2 在 使用 CAL之后,与CPU1之间的IPC 通讯卡死于 CPU1的 IpcPut 函数

    Part Number: TMS320F28377D

    当配置完CPU2 的Cla初始化函数之后 , CPU1 的IPC通讯函数卡死

    CPU2 IPC配置函数

    int counter = 0;
    EALLOW; // This is needed to write to EALLOW protected registers
    PieVectTable.IPC0_INT = &CPU01toCPU02IPC0IntHandler;
    PieVectTable.IPC1_INT = &CPU01t…

  • TMS320F280023-Q1: ECCN编码是多少

    Part Number: TMS320F280023-Q1

    请提供ECCN编码 谢谢

  • TMS320F28374S: 相同的编译器、相同的配置、完全一样的源代码,不同时间编译的Lib文件不一样

    Part Number: TMS320F28374S

    相同的编译器、相同的配置、完全一样的源代码,不同时间编译的Lib文件不一样。如何保证生成的LIb二进制相同,便于工程管理和差异比对

  • TMS320F280049: 两颗DSP通讯--CAN引脚直连

    Part Number: TMS320F280049

    想请教一下,

    两颗DSP的CAN通讯,不要  CAN收发器   的情况下,

    能否两颗DSP-CAN引脚直连,实现CAN通讯:

    DSP1---------DSP2

    CANTx ------CANRx

    CANRx ------CANTx

    还是说一定需要每颗DSP 的CAN必须要接一个收发器,连接到CAN总线

  • TMS320F28335: 在长时间没有上电后的第一次上电,ADC端口采集不正常

    Part Number: TMS320F28335

    平台:TMS320F28335
    问题描述:长时间没有给板子上电,第一次上电后其ADC采集到的电压不正常,之后的上电程序运行正常
    尝试过的手段:1、怀疑是实际端口电压确实存在问题,使用示波器采集端口电压发现实际电压很快到位的(大致50ms),程序中已经做了6S的延时处理,分别是外设初始化后延时5S,检测前延迟1S。
    2、怀疑是使用的PWM没有产生SOC信号导致ADC没有进行转换,在每一次发送ADC结果寄存器的原始数值前,手动触发一次ADC转换

    下图为上电第6秒后…

  • TMS320F28035: TI官方 有没有C2000MCU可以参考的AD7689的demo程序?

    Part Number: TMS320F28035
    Other Parts Discussed in Thread: C2000WARE
1 2 3 4 5 »