![]() |
资源:
|
为大学打包的 OMAP-L138/C6748 DSP 实验板套件 (TMDSEXPL138-UNV) 为学术机构提供开始教学和启动使用 TI TMS320C6000 DSP 的项目所需的全部内容。DSP 的 TI TMS320C6000 系列常用于实时 DSP 课程、信号和系统课程、DSP 理论实验室课程以及许多使用 DSP 的应用和项目(如电信)。用于大学的实验板套件是适于 OMAP-L138 的低成本灵活开发平台,OMAP-L138 是基于 C6748 DSP 和 ARM926EJ-S 32 位 RISC MPU 的低功耗双核处理器。
使用行业标准硬件和软件为学生提供动手实时 DSP 实验,比之单纯用理论和仿真来教学具有显著优势。该版本的实验板套件以及 TI 的 Code Composer Studio 集成开发环境 (IDE)(利用设备的 C6748 侧),为 DSP 提供了完整的工作站或项目设置。有关全面的 TMDSEXPL138-UNV 的文档、软件、教学材料和教科书,请访问 www.ti.com/EXPL138-UNV。
|
|
| 名称 | 器件型号 | 订购价格 | |
| 用于大学的 OMAP-L138/C6748 DSP 实验板套件 | TMDSEXPL138-UNV | $295.00 |
![]() |
The C6000 Teaching ROM is based on the TMS320C6748 installed in the OMAP-L138 eXperimenters board. The material is organized in four parts from basic to advance. Each part contains a set of presentations covering the relevant topics and a set of examples applying the concepts introduced in those topics. More info » |
|
![]() |
||
![]() |
This textbook teaches digital signal processing theory, MATLAB simulations and then shows how to use the results in real-time applications. More info » |
|
![]() |
||
![]() |
This is the most comprehensive text available for hands-on teaching of Digital Signal Processing, and the first book to feature the new floating point DSP development system, the OMAP-L138 eXperimenter and Code Composer Studio v4. Using a practical approach, the book provides a large number of real-time example programs that use actual input and output signals and give visible and audible results. It is an excellent teaching aid for professors wishing to teach DSP via laboratory experiments and for students or engineers wishing to study DSP using the inexpensive OMAP-L138 eXperimenter. More info » |
|
|
|
||||||||||||||