Other Parts Discussed in Thread: TUSB8041, TUSB8042, TUSB8044
你好
请问TUSB8041,TUSB8042,TUSB8044,这些芯片都有什么区别,望回复,谢谢!
1,PC与hub之间插入USB3.0线缆,然后再上电,能够正常识别下行端口的USB3.0设备。然后插拔上行端口的USB3.0设备,就无法识别下行端口的USB3.0设备。
2,USB2.0设备上电和插拔正常
3,在上电识别到下行USB3.0的情况下,插拔下行端口的USB.0设备,可以正常识别。
4,在1的基础上,插拔下行USB3.0设备,可以正常识别。
5,有的设备全部正常,有的设备会出现这个问题。
注:设备由外部电源供电,hub的3.3V比1.1V上电提前1…
When the CPU started,it can’t connect the USB HUB( TUSB8041) occasionally.
Restart the TUSB8041, sometimes it will work well, and sometimes the USB 2.0 will disconnect.
When the USB 2.0 disconnected, the CPU UART0 will print like this:
Compare above, when
…原理图见下图,现在SOC启动后给USB 5V供电,但是SOC不能识别芯片,现在怀疑芯片没有正常启动,有以下表现:
1.FULLPWRMGMTz/SMBA1/SS_UP配置为0,启动电源管理,PWRCTL_POL配置为高,但是PWRCTL*一直输出低电平
2.晶振激励电压在上电时是有的,并且在上电1.5ms后能正常起振,但是起振90ms之后激励电压消失
您好,使用TUSB8041RGCR扩展接口,结果下行接口无法识别。
请帮忙分析一下, 多谢!!!
1.配置接口用的SMBUS,上位机能扫到地址能读出寄存器内容,没有进行配置,均为默认设置。
2.上电时序现在有问题,3.3v先于1.1V先上的
3.连接器端供电正常 5V。
4.部分信号电平正常:USB_VBUS 0.5V GRSTZ 3.3V
5.如果上电的过程中将GRSTZ强制拉低,卡机后信息如下:
root@FHD3:~# lsusb
HI Sir
We have plan to implement TUSB8041 solution in our project.But we have not got TUSB8041EVM for pre-validation.
we found a issue by using oher manufacturer's HUB during our pre-validation.Please help to comfirm whether the TUSB8041…
使用TUSB8041 设计了一款 TYPE-C扩展坞 HDMI+ 4口 USB 3.0+RJ45 百M网口。 其中 4口 USB 3.0 +1 RJ45 百M网口 使用2片TUSB8041级连。 芯片方案: VL171+TUSB8041(X2)+CS5261+SR900AI.
使用是TYPE-C母口。USB3.0接口使用 TYPE-A母口
VL171 是接口双向换向芯片
TUSB8041 做USB3.0 HUB芯片,2片级连。芯片A使用3个下行USB3.0接口余1个下行USB3…
您好!TUSB8041-Q1 datasheet第15页8.3.7章节有如下说法:
Bus contention while VDD33 is powered up must be limited to 100 hours over the projected life-time of the device.
这句话应如何理解?意思是每隔100小时要重新给芯片来一次上电吗…
我想问一下USB Hub
1)是不是类似于模拟开关,是分时复用的?
2)Hub对Host一端和对Device一端都是同一个Speed, 例如USB3.0 Hub, 两端都是Super Speed?
答案是不是对所有USB Hub都通用,而不仅仅是本问题所选型号?
关于TUSB8041有AMI模型吗,我在官网没搜索到,有的话请发一下链接,谢谢。
1. TUSB4041和TUSB8041它们俩是通过I2C和SMBus接口和SOC进行通信么?参考电路中使用的是EEPROM,它是不需要上位机驱动么?
2. 如果作为I2C SLAVE与SOC进行通信它的器件地址是多少?
3.它内部的USB供电使能,是通过USB_D+/USB_D-来判断是否接入OTG设备?从而控制输出供电么?
TI的专家:
我在使用TUSB8041制作一款USB HUB控制板,在高温环境(50℃)时,USB3 TEST PLUG接在HUB板的3.0下行端口,HUB板的上行端口接在工控机上,用USB回环工具测试USB HUB板收发数据的功能;发现有掉线的情况
同时,TUSB8041下端级联TUSB4041扩展4个USB2.0接口,发现USB 2.0的下行接口在高温(50℃)也会掉线;并且级联的TUSB4041扩展4个USB2.0接口在高温高湿…
type_c_V1.0_REV.pdf 电路中USB3.0-HUB的Tusb8041芯片工作正常,USB3.0-HUB可以正常工作,我们可以通过USB3.0接口J31可以从U盘正确读写数据或文件,但TYPE-C型接口的USB3.0没有收发数据,无法工作,Tps25820dss芯片(u140)可以输出5V电压,TYPE-C型接口的USB2.0也可以工作,但TYPE-C接口的USB3…
采用8041做的hub,传输速率正常,只不过对线缆要求比较高,只能用质量比较好的线缆(或者粗缆),使用稍微差一点的线缆就会出现传输错误(距离8041越远的接口出错的频率越高)。这种问题主要是哪些情况导致的,板子是用的四层板。板子没有着重考虑阻抗匹配,不知道是否跟这个有关系。请大家给提提建议,谢谢!
hub不工作,down stream不识别,请帮忙分析原因?谢谢!
1,各power正常---VBUS:0.499V、VDD:1.1V、VDD33:3.3V
2,GRSTz为high
3,24MHz不起振
4,up stream为OTG(断开hub,OTG在host端可正常识别)
Ps.图中symbol value前缀为X_表示NC