dear:
we use the SN65DP159 for FPGA EVB,we want to 135MHz output!
and setting reg. as picture( flow the datasheet) but the result of refclk_out is 280MHz
how can we set the reg. to get 135MHz ?or should we set the others reg.?
…dear:
we use the SN65DP159 for FPGA EVB,we want to 135MHz output!
and setting reg. as picture( flow the datasheet) but the result of refclk_out is 280MHz
how can we set the reg. to get 135MHz ?or should we set the others reg.?
…参考xilinx的ZCU102相关设计,但是FPGA使用K7系列,结合自己的应用,没有使用DDC,HDP_SNK信号在我的设计中直接上拉到了3.3V,使用XILINX的HDMI核输出分辨率为1080p@60Hz分辨率视频。
在调试中,DP159输入信号的AC耦合前后断信号都有信号(时钟频率正确,为148.5MHz,时钟单端摆幅约为200mv),并参照xilinx的demo程序进行了配置,且配置后读取的值与预想配置的值一致。
但是在DP159的后端没有对应的波形输出…
Hi, 想麻煩幫忙確認TMDS181IRGZT & SN65DP159RGZT 設計.
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplified | Hungarian | Russian |
Chinese Traditiona… |
Q1:从调试HPD_SRC信号来看,当OE为低时,该信号为高,当OE为高时,该信号为低;是不是可以理解为OE为高,HPD_SRC为低时,是正常的可以传输视频流的?
A1:Q1已解决
Q2:比如我要配置0Bh寄存器,其中的bit[2]为Reserved,但是其它的bit是可以写入配置的,文档中有提到配置保留bit可以会产生意外情况,所以请问我这个对0Bh的[7:0]写入配置应该没有影响把?
Q3:关于TMDS_CLOCK_RATIO_STATUS字段的一些疑问…
① 写入和读出的寄存器数据不一致
② 读出过程中有的有应答,有的没有应答
以下是关于配置HDMI2.0的寄存器写入和读取的顺序,0-4为写入,5-9为读出对应写入的寄存器
[0]寄存器写入的实际波形图如下:
[1]寄存器写入的实际波形图如下:
[0]寄存器读出的实际波形图如下:为什么发送7位器件地址+1读标识没有应答?
[1]寄存器读出的实际波形图如下:为什么写入和读出的数据不一致?
现在是这样的,FPGA输出三路数据和一路时钟通道,其中数据速率为4.752Gbps,即HDMI2.0,现在需要对其进行配置然后传输
① 通过vivado中的HDMI输入输出demo,找到其中的dp159.c文件,不知是否按照其配置更改为verilog就可?
② 如何确定DP159是ZOMBIE还是ES器件,在我们的DP159背面,其丝印为DP159 TI 97I C7EZ G4,请问这个属于哪种器件
③ 由于没有SLLA359手册,所以我这边参考的是ZCU104demo中的dp159…
使用SN65DP159通过HDMI连接便携式显示器,显示功能正常,但是测量发现在开机过程和关机过程HDMI的4对儿差分信号有5.6V的电压尖峰,长期导致SN65DP159损坏,加不同型号共模电感和TVS无法抑制共模电压尖峰
使用其他板卡使用其他重定时器芯片连接至该便携式显示器,测量没有电压冲击,这种情况是否和SN65DP159模式配置有关?
SN65DP159RSBR使用HDMI转HDMI重定时,4对差分线采用直连的方式,OE 68K接3V3 , SDA_CTL 和SCL_CTL 接GND, I2C_EN/PIN 68K接地, SLEW_CTL 68K接3V3, PRE_SEL悬空, EQ_SEL/A0 悬空, HDMI_SEL/A1 68K接地。两端HDMI接显示器和电脑主板,发现无法正常显示,会是什么原因。
we new design HDMI 2.0 TX side used DP159 & TPD5S115YFFR
1.please revuew circuit.
2.If the access circuit, we are worried that the DDC capacitor exceeds Hhdmi_2.0_dp159_TX_OUTP_OK.pdfDMI SPEC 50PF,Can you help me confirm this…
你好,
我们目前在设计一款工控机产品,CPU采用Intel。若使用Intel DDI信号要输出HDMI 2.0(不做DP Dual mode),应该选用 RSB封装的就可以了吗?
请问有人用过SN65DP159吗?
DP1.2输入时是否支持HDCP1.4解密?
HDMI输出是否可以不进行HDCP的加密?
我的MCU通过SN65DP159的DDC通道读取显示器的EDID,始终读取不到,示波器测量,SN65DP159的LINK端DDC没有I2C信号,但是SN65DP159的SRC端是有DDC信号的。请问有哪些方面会导致DDC信号出问题?