HI,
Could you please inform me if there are strict requirements for the power-up voltage sequencing of AWRL6432? The power supply manufacturer I am consulting with requires matching its power-up sequence. I have only seen a diagram…
HI,
Could you please inform me if there are strict requirements for the power-up voltage sequencing of AWRL6432? The power supply manufacturer I am consulting with requires matching its power-up sequence. I have only seen a diagram…
Hello,
I have the following questions that I would like answered:
1. Generally speaking, when the chip is booted, the code and data of the external flash will be loaded into the code ram and data ram of the chip. In this chip, is…
您好,我使用DCA1000EVM_CLI_Control命令而不通过mmWaveStudio采集数据时,每次只能采集到2kb数据,我的采集步骤如下:
1. 通过DCA1000EVM_CLI_Control reset_ar_device和reset_fpga命令重置配置
2. 使用DCA1000EVM_CLI_Control fpga和record命令配置fpga,开启…
团队、
在研究频率特性时、我的客户发现、发射功率往往会从线性调频脉冲信号的开始到结束增加…
尊敬的 TI 团队
在编译源代码后加载调试映像时、会在特定地址中放置意外数据…
您好!
即使配置文件配置中的帧周期设置为330ms、其中预期帧速率为~ 3fps、但我们可以观察到~5fps。
请指导我们如何调试此问题、并告诉我们是否需要任何其他详细信息…
您好!
在 radar_toolbox_1_00_01_07…
https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1232497/awr2944-awr2944…