hello!
I have purchased the model TXS0108ENMER of your company.
When I measured the volume, I found that the thickness was not consistent with the PDF. I also found that the thickness was not consistent with the PDF when I bought…
hello!
I have purchased the model TXS0108ENMER of your company.
When I measured the volume, I found that the thickness was not consistent with the PDF. I also found that the thickness was not consistent with the PDF when I bought…
您好 Saurabh、
感谢您的快速回复。 iMX6UL 直接连接1.8V SDIO 线路。 其他行通过 TXS0108E 进行转换。 那么、使用 TXS0108E 对时间同步线路进行电平转换是合适的吗?
此致、Philipp
Hi TI team,
相关问题描述:
在使用TXS0108EPWR做SPI信号电平转换(1.8V与3.3V之间转换),转换前1.8V侧SPI信号回环测试速率可达到50M,
而3.3V侧SPI信号回环测试只能达到25M速率;
TXS0108EPWR芯片规格书宣称支持push-pull和open-drain两种模式,具体两种模式是如何实现的,电路上有何差异等等问题。
器件型号:TXS0108ENMER
封装尺寸最大高度与数据表不对应,请问这种情况是否存在误差值
尺寸数据表:download.siliconexpert.com/.../mpbgap4a.pdf
翻译
搜索
复制
您好、Albert、
嗯...这是一个非常奇怪的行为。 您有一些问题:
谢谢、
Arthur
下游负载当前未连接到任何器件、只需使用1M 探针监测输出即可。
附件是示波器快照、第一个探针探测芯片的开/关引脚、第二个探针探测芯片的 Vout。
开/关信号由 FPGA 驱动、但两者之间有一个1.5V 至3.3V 电平转换器(TXS0108E)。
最初、当系统上电但在对 FPGA 进行编程之前(大约0.8秒)、FPGA 将不会驱动信号(三态)、从电平转换器发出的信号将保持高电平大约0…
应用场景:VCCA=1.8V;VCCB=3.3V
1.在使用TXS0108EPWR做SPI信号电平转,转换前1.8V侧SPI信号回环测试速率可达到50M, 而转换后3.3V侧SPI信号回环测试只能达到25M速率,具体可能是什么原因。
2.TXS0108EPWR芯片规格书宣称支持push-pull和open-drain两种模式,具体两种模式是如何区分实现的,电路设计上有何差异?
3.(VCCA=1.8V)VIH定义为1.6V~1.8V以及VIL 定义为0V…
降级器、
数据表描述了: 电阻器的最小值由驱动器的拉电流能力决定。
我的 MCU 为 K60,IO 电流为25mA…
https://e2e.ti.com/support/logic-group/logic/f/logic-forum/726888/txs0108e-gate-bais-function
器件型号:TXS0108E栅极偏置‘s 功能?您能为我解释吗??
大家好、
我注意到、TXS0108中的 VIL 和 VIH 要求是 VCCI-0.2和0.15。
TXS0108的输出约为0.65*VCC…